Does Kinetis K60_100 support MII interface for ethernet connection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Kinetis K60_100 support MII interface for ethernet connection?

ソリューションへジャンプ
1,762件の閲覧回数
lucacampanale
Contributor I

I would like to use a Kinetis K60_100 mcu, MK60DN512VLL10.

In the K60 datasheet I read "Ethernet controller with MII and RMII interface to external PHY". But the phisical RX/TX pin to PHY are only two RXD0, RXD1 and TXD0,TXD1. It should be 0:3.

Indeed when I implement the Ethernet component on the Processor  Expert, selecting interface MII, I had the following error: "target processor does not contain peripheral".

What I do not understand?

Bless you !

ラベル(1)
0 件の賞賛
返信
1 解決策
1,618件の閲覧回数
mjbcswitzerland
Specialist V

Luca

The K60 supports MII Ethernet connection but you will need to chose a package with 144 pins for these options to be available.

The 100 and 121 pin packages lead-out only the RMII pins.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K60: http://www.utasker.com/kinetis/TWR-K60N512.html / http://www.utasker.com/kinetis/TWR-K60D100M.html / http://www.utasker.com/kinetis/TWR-K60F120M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,619件の閲覧回数
mjbcswitzerland
Specialist V

Luca

The K60 supports MII Ethernet connection but you will need to chose a package with 144 pins for these options to be available.

The 100 and 121 pin packages lead-out only the RMII pins.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K60: http://www.utasker.com/kinetis/TWR-K60N512.html / http://www.utasker.com/kinetis/TWR-K60D100M.html / http://www.utasker.com/kinetis/TWR-K60F120M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 件の賞賛
返信