Does K70 fully support the EMV spec ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does K70 fully support the EMV spec ?

Jump to solution
1,727 Views
youjongan
Contributor I

Dear Community..

Currently, i use the K70 MCU in my project and use the UART0 to control the IC card.

I want to know that K70 is fully supported on EMV spec (Level 1).

if the K70 is any limitations in order to pass EMV certification, please share the detailed information about it. 

Specially, on ISO7816 T=1 mode, Does it possible to support  the 11 etu ?

(11 etu should be support in order to pass EMV. )

if not supported, please tell me any solution.

Thanks

Yoo.

Labels (1)
0 Kudos
Reply
1 Solution
1,632 Views
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

View solution in original post

0 Kudos
Reply
1 Reply
1,633 Views
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

0 Kudos
Reply