Does K70 fully support the EMV spec ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does K70 fully support the EMV spec ?

ソリューションへジャンプ
1,698件の閲覧回数
youjongan
Contributor I

Dear Community..

Currently, i use the K70 MCU in my project and use the UART0 to control the IC card.

I want to know that K70 is fully supported on EMV spec (Level 1).

if the K70 is any limitations in order to pass EMV certification, please share the detailed information about it. 

Specially, on ISO7816 T=1 mode, Does it possible to support  the 11 etu ?

(11 etu should be support in order to pass EMV. )

if not supported, please tell me any solution.

Thanks

Yoo.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,603件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,604件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Yoo

Yes, the K70 really support  ISO7816(EMV Lv1). And unfortunately it does not support 11 etu.

0 件の賞賛
返信