Does Freesacle provide a library for fixed point math similar to TI IQMath?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does Freesacle provide a library for fixed point math similar to TI IQMath?

2,810 次查看
andreag
Contributor II

if not can someone suggest the easiest/most efficient (execution-wise) way to implement this in Kinetis seires MCU?

Thanks!

标签 (1)
0 项奖励
回复
3 回复数

1,810 次查看
eduardo_viramon
NXP Employee
NXP Employee

The Embedded Software and Motor Control libraries are probably what you're looking for, check them out here:

Embedded Software and Motor Control Libraries Product Summary Page

0 项奖励
回复

1,810 次查看
andreag
Contributor II

Hi guys,

thanks for the replies!

I amu sing a Kinetis L series (Cortex M0) so using floating point is not an option for any real time work. Also the motor control library is not available for this MCU (only for Cortex M4).

There are a few generic fixed point math libraries, but none seem to have the ease of use of the TI one. For real time control (in my case motor control) it is extremely useful and is probably the part I miss the most from TI...In particular CMSIS library is OK and I will try and use that first, but it does not have much in terms of fixed point math basic functions (conversions, basic operations, etc....)

Thanks for your help!

0 项奖励
回复

1,810 次查看
chris_brown
NXP Employee
NXP Employee

Hi Andrea,

I am not aware of any library that Freescale provides.  For standard floating point math, you should just be able to include math.h, declare float variables, and perform the math.  That library should be a part of most IDEs.  For more complicated functions (like computation of trigonometric functions, matrix math, vector math, filtering functions, etc.,), I suggest trying the ARM CMSIS DSP library. 

Hope this helps,

Chris

0 项奖励
回复