Does FRDMCD1020 work with Windows 10? How is the FRDM board programmed with SPIGen?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does FRDMCD1020 work with Windows 10? How is the FRDM board programmed with SPIGen?

ソリューションへジャンプ
2,061件の閲覧回数
PB123
Contributor II
0 件の賞賛
返信
1 解決策
1,961件の閲覧回数
PB123
Contributor II

What I have discovered is that the Freedom Boards KL25Z bootloader was reset by pushing the RESET and powering the board with USB.  When you loose the Bootloader, Windows 10 does not allow user to reprogram the bootloader.  I have not found a way around this yet.  

Users must first load the drivers and then plug into the USB only.  Don't use the reset or bootloader usb port.  

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,962件の閲覧回数
PB123
Contributor II

What I have discovered is that the Freedom Boards KL25Z bootloader was reset by pushing the RESET and powering the board with USB.  When you loose the Bootloader, Windows 10 does not allow user to reprogram the bootloader.  I have not found a way around this yet.  

Users must first load the drivers and then plug into the USB only.  Don't use the reset or bootloader usb port.  

0 件の賞賛
返信
2,019件の閲覧回数
PB123
Contributor II

Thank you for the response, however when I plug in the Freedom board to PC USB and load SPIGen application I get the error message 

"The SPI Dongle was not detected" 

When the Freedom board is plugged into the PC, there is no "New Hardware Detected" message from the PC.  

0 件の賞賛
返信
1,997件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Change your PC to test again.

 

0 件の賞賛
返信
2,033件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Yes,it supports the WIN10.

For the detail operation please see below link user manual from page14:

KTFRDMCD1020EVMUG, FRDMCD1020EVM evaluation board - User's Guide (nxp.com.cn)

0 件の賞賛
返信