Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.

2,935 Views
larryhe
Contributor I
0 Kudos
Reply
6 Replies

2,769 Views
larryhe
Contributor I

I decide to select MK22FN512 to use its parallel bus (Flexbus). my question is fixed.

0 Kudos
Reply

2,769 Views
miduo
NXP Employee
NXP Employee

Hi,

So at present, the 32 bit SPI is a bottleneck. Please make reference from the thread below:Transmit 32 Bit via SPI . Hope it is helpful.

0 Kudos
Reply

2,769 Views
larryhe
Contributor I

Yes this is a way, but your solution will need CPU involvement frequently..

some 16-bit ADC or DAC needs 24-bit CMD/data in one SPI CS period.

My assumption is: start the SPI then CPU go to deal other works. uC works efficiently.

May you tell me your a few of your uC's which are capable of 32-bit SPI but low cost?

0 Kudos
Reply

2,769 Views
alexeyusoltsev
Contributor IV

Hi Larry!

If you dont want to interact with the processor you can use DMA.

Anyway max SPI speed is the BUS/2 and 1 trasnsaction(8 bit) is BUS/16 that will not demand a lot of CPU power. Even more you have an FIFO on both TX and RX so you can put your 24 bit data there and wait for tx-interrupt that will lead to BUS/48 in the interrupt mode.

MKL 26 is a good choice-low cost and it' USB is crystalless.

I hope it help,

Regards Alexey.

0 Kudos
Reply

2,769 Views
mr_max
Contributor IV

Why do you need 32 bits SPI ? You can just send 4 bytes and manually control SS or CS pin with a dedicated gpio.

0 Kudos
Reply

2,769 Views
larryhe
Contributor I

I know you KL2 series has USB, but its SPI is 8 bits.

0 Kudos
Reply