Do I need TWR-SER board to run SPO2 demo with K53 MCU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do I need TWR-SER board to run SPO2 demo with K53 MCU?

1,223 Views
johnodonnell
Contributor I

I have already purchased K53N512 MCU board and MED-SPO2 pulse oximeter dev kit.   Do I also need TWR-SER in order to run the SPO2 demo as suggested in AN4327?  It seems strange because K53 board already has a USB port for IAR debugging and serial communication?

Labels (1)
0 Kudos
Reply
1 Reply

1,101 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi John,

Yes, you will need the TWR-SER board to run the MED-SPO2 demo since the demo uses the TWR-SER USB port to communicate with the GUI. The OSBDM debug port in the K53 board is used to download the program to the MCU using IAR and after this you will have to connect the TWR-SER to the host computer.

You can find more information on the following link:

http://cache.nxp.com/files/32bit/doc/ref_manual/DRM141.pdf

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply