Do not working ethernet with kinetis K64 with KSZ8081RNACA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do not working ethernet with kinetis K64 with KSZ8081RNACA

3,937 次查看
VilemZ
NXP Employee
NXP Employee

Hi everyone,

I have working software on FRDM K64 and I tried make own hardware - I inspired from FRDM K64 schematic. Now, I have issue with connection ethernet. Schematic is on attachment. 

I tried read registers from KSZ8081RNACA - it is OK. When I connected cable, then it is not see any change. Any change on registers, any change on router. 

Please, could you help me, how can I debug it and find issue?

Thank you

Vilem

标记 (3)
4 回复数

3,600 次查看
VilemZ
NXP Employee
NXP Employee

I tried change XTAL for PHY (25 MHz). It is OK. When xtal is not soldered on board, then kinetis not working too, because I am using 120 MHz clock for kinetis. 

Now, I don't know, what have I do? Please help.

0 项奖励
回复

3,600 次查看
kazukiyamashita
Contributor II

I was troubled because LAN was not stable. Thanks and it worked.

Thank you for your help!

0 项奖励
回复

3,600 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think the hardware connection is okay. But pls check that the pin24 of KSZ8081 is Reset pin, you should connect a RC circuit as the FRDM-K64. For the connector of Ethernet, Pls check if there should be serial resistor for the LEDG- and LEDG+.

Hope it can help you

BR

XiangJun Rong

3,600 次查看
VilemZ
NXP Employee
NXP Employee

Hi,

thanks for your reply. When I compare schematic with FRDM k64F, then I don't see any RC circuit on the pin24 of KSZ8081. 

And serial resistor for the LEDG can't affect detection of cable. And I think, that it is clear.

Best Regards,

Vilem

0 项奖励
回复