Disabling External PullUp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Disabling External PullUp

2,399 次查看
infinity
Contributor I

I'm learning about MQX... but I have a simple problem... how can I change the registry to disable internal pull-up for a GPIO?

 

I'm using PORTC_PCR10 as digital input.

 

Thank you.

0 项奖励
回复
3 回复数

2,105 次查看
mjbcswitzerland
Specialist V

Hi

 

Is this not a question for the Kinetis?

 

The Coldfires have fixed internal pullups (where present) which are enabled by default.

 

The Kinetis allows configuration of pull-up/down or none.

If you write 0x00000100 to the corresponding PCR register the pin will be configured as GPIO - as input it has no pullup/down.

The pullup/down is only enabled when 0x00000002 is set as well whereby the bit 0x00000001 controls whether this is pullup or pull down.

 

Regards

 

Mark

 

0 项奖励
回复

2,105 次查看
infinity
Contributor I

Oh yes it is true, I put the post in the wrong section. 

I'm using TWRK40_512.

How do I move my post? Please some admin can do this for me?

But I still have problems, I set as you said PORTC_PCR10. 

But it seems that there is some function call that overwrite this setting and then reactivate the pull-up ... why this behavior?

0 项奖励
回复

2,105 次查看
mjbcswitzerland
Specialist V

Hi

 

This sounds like a software issue so it depends on the SW that you are using.

 

1) Try puttiung a breakpoint on write accesses to the register to see where it is being written from

2) Or, write the value that you want later (after the unknown function has done its work).

 

Regards

 

 Mark

 

0 项奖励
回复