Differences between NXP Kinetis MK20DN512ZVLQ10 and NXP Kinetis MK20DN512VLQ10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differences between NXP Kinetis MK20DN512ZVLQ10 and NXP Kinetis MK20DN512VLQ10

ソリューションへジャンプ
2,514件の閲覧回数
mickibiz
Contributor I

Hi,

I would like to know if there are any significant electrical and mechanical differences between NXP Kinetis MK20DN512ZVLQ10 and NXP Kinetis MK20DN512VLQ10.

A long time ago we developed several firmwares for NXP Kinetis MK20DN512ZVLQ10 - are these source codes fully compatible with NXP Kinetis MK20DN512VLQ10?

 

Thanks in advance.

Best regards,

Michele

0 件の賞賛
返信
1 解決策
2,499件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Michele,

These source codes are not fully compatible with NXP Kinetis MK20DN512VLQ10.
For the difference please refer: AN4445 Kinetis® K 100MHz Rev 1.x to Rev 2.x Migration Guide (REV 1)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,500件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Michele,

These source codes are not fully compatible with NXP Kinetis MK20DN512VLQ10.
For the difference please refer: AN4445 Kinetis® K 100MHz Rev 1.x to Rev 2.x Migration Guide (REV 1)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,505件の閲覧回数
myke_predko
Senior Contributor III

@mickibiz 

I bellieve the short answer to your question is "yes" they are compatible - just looking up the parts, the MK20DN512ZVLQ10 is noted as "Not recommended for new designs".  

Regardless, doing a quick scan of the distributors, it doesn't look like any of the MK20DN512VLQ10 are available and there doesn't seem any date on when they will become available so the more important question may be what 144 pin Kinetis parts *are* available or will be available soonest - which will mean changes to your software and maybe hardware.  

Stupid Covid.  

0 件の賞賛
返信