Difference between MK70FN1M0VMJ12 and PK70FN1M0VMJ12-ND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MK70FN1M0VMJ12 and PK70FN1M0VMJ12-ND

Jump to solution
1,601 Views
joelesco
Contributor III

Hi !

My question is a bit stupid but is there a difference between this 2 MCU ? The P before K70 means proto ?

Thanks a lot ! !

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,453 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

Pxx instead of Mxx means basically that is an early part and the part probably has not qualified for full production. It is normal that you can find Pxxx parts in the first development boards until the device  is fully qualified and in full production. The differences between P an M products can vary from one part # to the other. But technically is the same product if they have the same silicon mask version. For example part# with Pxx could have been only tested in a narrow temperature range. So a Pxx part can be exactly the same than Mxxx part but the qualification process could not be complete at the time of manufacturing the part.

I hope this helps.

Luis

View solution in original post

0 Kudos
Reply
1 Reply
1,454 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

Pxx instead of Mxx means basically that is an early part and the part probably has not qualified for full production. It is normal that you can find Pxxx parts in the first development boards until the device  is fully qualified and in full production. The differences between P an M products can vary from one part # to the other. But technically is the same product if they have the same silicon mask version. For example part# with Pxx could have been only tested in a narrow temperature range. So a Pxx part can be exactly the same than Mxxx part but the qualification process could not be complete at the time of manufacturing the part.

I hope this helps.

Luis

0 Kudos
Reply