Difference between MK70FN1M0VMJ12 and PK70FN1M0VMJ12-ND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between MK70FN1M0VMJ12 and PK70FN1M0VMJ12-ND

跳至解决方案
1,049 次查看
joelesco
Contributor III

Hi !

My question is a bit stupid but is there a difference between this 2 MCU ? The P before K70 means proto ?

Thanks a lot ! !

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
901 次查看
LuisCasado
NXP Employee
NXP Employee

Hi,

Pxx instead of Mxx means basically that is an early part and the part probably has not qualified for full production. It is normal that you can find Pxxx parts in the first development boards until the device  is fully qualified and in full production. The differences between P an M products can vary from one part # to the other. But technically is the same product if they have the same silicon mask version. For example part# with Pxx could have been only tested in a narrow temperature range. So a Pxx part can be exactly the same than Mxxx part but the qualification process could not be complete at the time of manufacturing the part.

I hope this helps.

Luis

在原帖中查看解决方案

0 项奖励
回复
1 回复
902 次查看
LuisCasado
NXP Employee
NXP Employee

Hi,

Pxx instead of Mxx means basically that is an early part and the part probably has not qualified for full production. It is normal that you can find Pxxx parts in the first development boards until the device  is fully qualified and in full production. The differences between P an M products can vary from one part # to the other. But technically is the same product if they have the same silicon mask version. For example part# with Pxx could have been only tested in a narrow temperature range. So a Pxx part can be exactly the same than Mxxx part but the qualification process could not be complete at the time of manufacturing the part.

I hope this helps.

Luis

0 项奖励
回复