Device is secure problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device is secure problem

1,896 Views
yusupkhan
Contributor II

Dear All,

Sometime we try to program newly assembled board using the Multilink we get this error inside CodeWarrior:

"Device is secure. Erase to unsecure?"

We are using MKL16. Some boards are working fine and some boards are showing error("Device is secure. Erase to unsecure?").

How to recover from this problem?

Matter is very urgent. Guide us.

Regards Yusup

0 Kudos
Reply
2 Replies

1,734 Views
BlackNight
NXP Employee
NXP Employee

Hi Yusup,

That message shows up as well if you connect to the wrong board/device, see https://mcuoneclipse.com/2012/05/28/device-is-secure/ .

Did you accidentially secure your device? As long as you do not have the 'disable mass erase' bit set, you always can erase it to unsecure it, see https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/  and https://mcuoneclipse.com/2014/06/22/preventing-reverse-engineering-enabling-flash-security/ .

I hope this helps,

Erich

0 Kudos
Reply

1,734 Views
yusupkhan
Contributor II

Thank you Mr.Erich. We will check and let you know.

Best regards,

Yusup Khan

0 Kudos
Reply