Detection distance USB ZigBee Packet Sniffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Detection distance USB ZigBee Packet Sniffer

1,761件の閲覧回数
k_vanderheiden
Contributor I

I am about to use the USB-KW24D512 as a ZigBee packet sniffer. Can someone tell me (theoretically or by experience) what would be max distance the sniffer will detect packets? (Indoor and outdoor)

Thanks!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,609件の閲覧回数
AngelC
Senior Contributor I

Dear K. van der Heiden,

The sniffer itself has a RX sensitivity of around –100 dBm, so it could still receive signals of such energy level. However, the maximum distance would depend more in the devices transmitting and the output power they are capable to achieve.

Between two USB-KW24D512 boards you will be able to transmit and receive within 30 meters indoors approximately. However, if another device (bigger antenna, printed antenna, power amplifier, etc.) has the ability to transmit to a long distance (i.e. TWRKW2x boards could achieve around +8dBm), the sniffer would still detect the packets from tens to hundreds of meters.

In brief, as long as the transmitted signal has enough energy, it will be detected and received by the USB-KW24D512.

Regards,

AngelC

1,609件の閲覧回数
k_vanderheiden
Contributor I

Ok, this information is what I need for now. Thanks for you reply, AngleC!

0 件の賞賛
返信