Default Core Clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Default Core Clock

2,290 次查看
mithunp_s
Contributor III

Hi All,

I'm using PT60 & FRDM board,

Once I create a bare board project in CW for any of these device (S08, KL) I want to know what will be default Core Clock codewarrior sets.

I know how to set particular clock frequency in both PE & nonPE projects,  but I want to know in bare board project what will be default setting once project is created, where can find these settings in project and can I directly modify these settings as per my requirement.

Rgds

Mithun

0 项奖励
回复
4 回复数

2,098 次查看
JimDon
Senior Contributor III

Also, if you use PE to set the clocks, you can see exactly what the clocks will be and how to set it there.

0 项奖励
回复

2,098 次查看
adriansc
Contributor IV

Hi,

For KL CW does not code this configuration, MCG comes out the reset in FEI (FLL Engaged Internal) mode (as Jim Donelson said) and you need to add code in order to change MCG modes. Check MCG mode state diagram:

Default core clock 1.png

It applies the same for S08 device: FEI is the default mode of operation for ICS; and CW does not code it.

Default core clock 2.png

Hope this helps.

0 项奖励
回复

2,098 次查看
Monica
Senior Contributor III

Mithun, how is it going?

Please keep us posted :smileywink:

Monica

0 项奖励
回复

2,098 次查看
JimDon
Senior Contributor III

>in bare board project what will be default setting once project is created, where can find these settings in project and can I directly modify these settings as per my requirement.

There are no settings for the clock (or anything else like that) in a bare board project. You need to add code for this.

This may apply to all Kinetis chips:

25.5.2 Using a 32.768 kHz Reference

"In FEE and FBE modes, if using a 32.768 kHz external reference, at the default FLL

multiplication factor of 640, the DCO output (MCGFLLCLK) frequency is 20.97 MHz at

low-range."

0 项奖励
回复