Debugging issue with KEA128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugging issue with KEA128

跳至解决方案
5,305 次查看
0815
Contributor II

I have an heavy debug issue with a custom designed KEA128 board:

After starting the debugger I'm not able to step through the program (F5 or F6). I'm using the PE Multilink Universal Debugger and the S32 Design Studio with PE plugin. On other workspaces and the same toolchain the debugging works flawlessly. I'm running into a similar issue if I try to debug this workspace on a TRK-KEA128 evaluation board via OpenSDA. So it seems this issue has something to do with this projects workspace.

Here is what I'm getting in the console windows:

GNU gdb (GNU Tools for ARM Embedded Processors) 7.8.1.20141128-cvs

Copyright (C) 2014 Free Software Foundation, Inc.

License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.  Type "show copying"

and "show warranty" for details.

This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".

Type "show configuration" for configuration details.

For bug reporting instructions, please see:

<http://www.gnu.org/software/gdb/bugs/>.

Find the GDB manual and other documentation resources online at:

<http://www.gnu.org/software/gdb/documentation/>.

For help, type "help".

Type "apropos word" to search for commands related to "word".

monitor preserve0 0

monitor selectcore 0

continue

Continuing.

Note: automatically using hardware breakpoints for read-only addresses.

Temporary breakpoint 1, main () at ../source/main.cpp:53

53 PE_low_level_init();

No breakpoint number 1.

and

Connection from "127.0.0.1" via 127.0.0.1

Copyright 2012 P&E Microcomputer Systems,Inc.

Command Line :C:\Freescale\S32_ARM_v1.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.2.5.201511061812\win32\pegdbserver_console -device=Freescale_KEx_S9KEAZ128M4 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=5000 -port=US

CMD>RE

Initializing.

Target has been RESET and is active.

CMD>CM C:\Freescale\S32_ARM_v1.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.2.5.201511061812\win32\gdi\P&E\supportFiles_ARM\Freescale\KEx\freescale_s9keaz128m4_pflash.arp

Initializing.

Initialized.

;version 1.03, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [ke_128k_pflash_ftmre_m0]

;device freescale, s9keaz128m4, pflash

;begin_cs device=$00000000, length=$00020000, ram=$20000000

Loading programming algorithm ...

Done.

CMD>EM

Erasing.

Module has been erased.

Initializing.

Initialized.

;version 1.03, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [ke_128k_pflash_ftmre_m0]

;device freescale, s9keaz128m4, pflash

;begin_cs device=$00000000, length=$00020000, ram=$20000000

Loading programming algorithm ...

Done.

CMD>PM

Programming.

Processing Object File Data ...

                               

.

Programmed.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00000000-000000BF ...

Ok.

   block 00000400-0000BBCF ...

Ok.

   Checksum Verification Successful. (Cumulative CRC-16=$FF3B)

CMD>RE

Initializing.

Target has been RESET and is active.

Preset breakpoint encountered.

Any ideas?

Thanks in advance!

标记 (3)
1 解答
4,929 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi 0815,

Please make sure you didn't select "Skip all breakpoints" button:

pastedImage_0.png

And then try removing all breakpoints and setting a new one.

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,188 次查看
Lukas_Frank
Senior Contributor I

Hi Dear @Carlos_Mendoza ,

 

I have same issue. How did you solve it?

 

Here is my issue:

https://community.nxp.com/t5/i-MX-RT/IMXRT1064-PEMicro-Debug-Error-During-Flash-Programming/m-p/1590...

 

Thank you.

0 项奖励
回复
4,175 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi @Lukas_Frank ,

 

Is this the first time you load a demo application into the board? Please make sure that your board is configured for internal boot and not for serial downloader mode.

 

Regards,

Carlos Mendoza

 

 

4,159 次查看
Lukas_Frank
Senior Contributor I

Hi Dear @Carlos_Mendoza ,

 

I used internal boot mode as you mentioned. But I think the issue related with my debug configuration. I am using J34 in EVK. But I think I need to use LPC-Link2 Debug Probe for debugging with J34. Could you please clarify me about Am I able to debug with J34 or not? Because reference manual says below and I thought that I will be able to debug my card with J34 if I use FreeLink Interface's JTAG connector. Does this JTAG Connector supports debugging?

 

First Clue:

FreeLink_Interface_High_Speed_JTAG_2.pngFreeLink_Interface_High_Speed_JTAG_2.png

 

Second Clue:

FreeLink_Interface_High_Speed_JTAG.pngFreeLink_Interface_High_Speed_JTAG.png

 

Thanks for your help.

0 项奖励
回复
4,930 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi 0815,

Please make sure you didn't select "Skip all breakpoints" button:

pastedImage_0.png

And then try removing all breakpoints and setting a new one.

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,929 次查看
0815
Contributor II

You are right, it is embarrassing. :smileyblush: