Hello @Mr7 ,
Thanks for your post. I did a test on my evb board, with no problem.

However, I noticed that the orange LED D2 stays ON instead of LED D9.
Please check my status under MSD, which should be mounted with the name TWR-KM35(D:), instead of showing "maintenance".

Please refer the DAPLink bootloader update | Mbed to check.

When your device mount with the name "maintenance", you need install the DAPLink interface application, just open the device's root directory then drag-and-drop the firmware update into this directory. The firmware is attached.

Hope it can help you.
BRs,
Celeste
-------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-------------------------------------------------------------------------------------------