DSPI slave example on FRDM-K66F like board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSPI slave example on FRDM-K66F like board

Jump to solution
2,175 Views
mdecandia
Contributor III

Hi all,

we are testing the dspi samples from SDK and they are not working on a board derived from FRDM-K66F.  There are few changes (clock frequencies, pinmuxing) but they should not impact SPI slave functionality.

Do they  should work on this evb?

 

Michele

0 Kudos
Reply
1 Solution
2,136 Views
mdecandia
Contributor III

Hi @RaRo,

thanks for your feedback. In the meanwhile we have found the issue: we were using the SPI0_PCS5 as chip select pin that cannot be used as SPI slave.

Kind regards.

Michele

 

View solution in original post

0 Kudos
Reply
2 Replies
2,137 Views
mdecandia
Contributor III

Hi @RaRo,

thanks for your feedback. In the meanwhile we have found the issue: we were using the SPI0_PCS5 as chip select pin that cannot be used as SPI slave.

Kind regards.

Michele

 

0 Kudos
Reply
2,140 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @mdecandia,

Could you please help us with more information related with your issue? Did you receive an error while debugging or your problem is that the communication is not working? Could you tell us which other changes did you make in your board? What clock frequency are you working with? What pins do you configure for the DSPI you are working with? Which SDK example and version are you using?

Best regards, Raul.

0 Kudos
Reply