DMA 'always on' source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DMA 'always on' source

跳至解决方案
3,426 次查看
patricio
Contributor IV

Hello, 

I am having some difficuties with the DMA, and I would appreciate if somebody could help with the following doubts:

1) What should be the  source to be choosed in a channel, if the request is comming from the major loop link of the previous channel? Any of the differents 'always on' source?

2) At the end of the following post, Help - continuous DMA with PIT , it says that there was a bug in the silicon when using PIT wiht 'always enabled' request. Is it fixed already?

Thanks for your help. 

1 解答
3,307 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

I've not found this bug record in errata of K64_120, so I think this errata is fixed now.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
3,307 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What should be the  source to be choosed in a channel, if the request is comming from the major loop link of the previous channel? Any of the differents 'always on' source?
-- Yes, any one of 'always on' sources is Ok.
 2) At the end of the following post, Help - continuous DMA with PIT , it says that there was a bug in the silicon when using PIT wiht 'always enabled' request. Is it fixed already?
-- Before answering your question, I think you'd better tell me which chip you use.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,307 次查看
patricio
Contributor IV

Hi Jeremyzhou,

I am using K64FN1M0M12, in the TWR-K64 board. 

Thank you for your help. 

Best regards. 

0 项奖励
回复
3,308 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

I've not found this bug record in errata of K64_120, so I think this errata is fixed now.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,307 次查看
patricio
Contributor IV

Hi Jeremyzhou,

I appreciate your quick response. 

Thank you. 

0 项奖励
回复