DMA 'always on' source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA 'always on' source

ソリューションへジャンプ
3,387件の閲覧回数
patricio
Contributor IV

Hello, 

I am having some difficuties with the DMA, and I would appreciate if somebody could help with the following doubts:

1) What should be the  source to be choosed in a channel, if the request is comming from the major loop link of the previous channel? Any of the differents 'always on' source?

2) At the end of the following post, Help - continuous DMA with PIT , it says that there was a bug in the silicon when using PIT wiht 'always enabled' request. Is it fixed already?

Thanks for your help. 

1 解決策
3,268件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

I've not found this bug record in errata of K64_120, so I think this errata is fixed now.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
3,268件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What should be the  source to be choosed in a channel, if the request is comming from the major loop link of the previous channel? Any of the differents 'always on' source?
-- Yes, any one of 'always on' sources is Ok.
 2) At the end of the following post, Help - continuous DMA with PIT , it says that there was a bug in the silicon when using PIT wiht 'always enabled' request. Is it fixed already?
-- Before answering your question, I think you'd better tell me which chip you use.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,268件の閲覧回数
patricio
Contributor IV

Hi Jeremyzhou,

I am using K64FN1M0M12, in the TWR-K64 board. 

Thank you for your help. 

Best regards. 

0 件の賞賛
返信
3,269件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi AITOR ARANZABAL,

I've not found this bug record in errata of K64_120, so I think this errata is fixed now.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,268件の閲覧回数
patricio
Contributor IV

Hi Jeremyzhou,

I appreciate your quick response. 

Thank you. 

0 件の賞賛
返信