DM-K22F board not booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DM-K22F board not booting

1,445件の閲覧回数
mikef1
Contributor I

I recently received my frdm-k22f module from a distributor.  When I plug it in, it does not behave like it should according to the quick start guide, so I assume that it has old software on it. The problem is, i can not even putty into the board, from my windows10 machine, it keeps outputting a text file that says "timed out". Is there anyway around this? I read that it may require a windows7 machine to boot, but I don't have any of these around anymore...

ラベル(3)
0 件の賞賛
返信
1 返信

1,358件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

You can refer to this post if you don’t have access to a machine with windows 7.

https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/

Best regards,

Ivan.

0 件の賞賛
返信