DFU bootloader recieving 1024 FS transactions issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DFU bootloader recieving 1024 FS transactions issue

1,561 次查看
michael_keezer
Contributor I

DFU bootloader question. I currently have an issue with using the LONG_RECIEVE_TRANSACTION define. If the set this define my setup stage and all my 1K byte data transfers is received wt ACK (note I'm the DEVICE) but the status stage data is not sent and all I see is NAK being sent by the SIE. If I turn off the define and set it back to 64 byte it works. What is missing for LONG_RECIEVE_TRANSACTION to work? is there any new updates to the DFU bootloader code?

0 项奖励
回复
2 回复数

1,449 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following document, you will find information for your reference. 

Bootloader demo steup - USB DFU.pdf 


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,449 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Can you please tell us the device that you are using?

0 项奖励
回复