DDR Controller on K70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR Controller on K70

2,004件の閲覧回数
massimoballerin
Contributor II

We have to interface a K70FN1M0VMJ12 an external DDR memory. I've seen that are not supplied configuration tool for the controller or sample source code of SDK, at least for the Kinetis K series, or am I wrong? You know tell me the best way for the use of this controller on K70?

ラベル(1)
タグ(5)
1 返信

1,701件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

We have the DDR init tool that is for K70. There are three memory types supported - DDR1, LPDDR1 and DDR2. Also, we have 9 of the three memory types validated in our validation boards. User can base on one the memory type or template to start with. The tool can only generate c code. CW and IAR will be supported later.

http://cache.nxp.com/files/32bit/software_tools/initialization/boot_code_generation/KINETIS_K70_DDR_...