Crystals and oscillator parts used in FRDM-K22F board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crystals and oscillator parts used in FRDM-K22F board

Jump to solution
1,746 Views
vishalgirisagar
Contributor II

Hi All,

  I am using K22F board. I have tested a prototype of my software on this board. And it works completely. Now I am in next stage of building my own board using the same MCU. I am stuck with oscillators and crystals used. I want to used both RTC crystal (32.768KHz) and 8Mhz crystal. From the schematics, I see the following.

pastedImage_0.png

pastedImage_1.png

  I have no clue how to use the crystals and oscillators. I tried to find the component names of these, but google did not help. It will be great if some one could tell me which components are used in the board.

Thanks in advance.

Tags (3)
0 Kudos
Reply
1 Solution
3 Replies
1,563 Views
cutworth_wang
Contributor II
0 Kudos
Reply
1,560 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Vishai

For 32.768KHz, R85 is DNP.

For 8MHz, R57 is need.

Best Regards

Paul

0 Kudos
Reply
1,560 Views
vishalgirisagar
Contributor II

Hi Zhe Tian,

I checked the data sheet of the crystal.

http://sg.element14.com/abracon/abm3b-8-000mhz-b2-t/crystal-8mhz-18pf-5-x-3-2mm/dp/2368190

According to the datasheet, the required Resistance is 200 ohms. But in the schematics of Freescale board, they have used 1M resistance. Can you please clarify on this?

0 Kudos
Reply