Crystals and oscillator parts used in FRDM-K22F board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Crystals and oscillator parts used in FRDM-K22F board

跳至解决方案
1,753 次查看
vishalgirisagar
Contributor II

Hi All,

  I am using K22F board. I have tested a prototype of my software on this board. And it works completely. Now I am in next stage of building my own board using the same MCU. I am stuck with oscillators and crystals used. I want to used both RTC crystal (32.768KHz) and 8Mhz crystal. From the schematics, I see the following.

pastedImage_0.png

pastedImage_1.png

  I have no clue how to use the crystals and oscillators. I tried to find the component names of these, but google did not help. It will be great if some one could tell me which components are used in the board.

Thanks in advance.

标记 (3)
0 项奖励
回复
1 解答
1,569 次查看
cutworth_wang
Contributor II
0 项奖励
回复
3 回复数
1,570 次查看
cutworth_wang
Contributor II
0 项奖励
回复
1,567 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Vishai

For 32.768KHz, R85 is DNP.

For 8MHz, R57 is need.

Best Regards

Paul

0 项奖励
回复
1,567 次查看
vishalgirisagar
Contributor II

Hi Zhe Tian,

I checked the data sheet of the crystal.

http://sg.element14.com/abracon/abm3b-8-000mhz-b2-t/crystal-8mhz-18pf-5-x-3-2mm/dp/2368190

According to the datasheet, the required Resistance is 200 ohms. But in the schematics of Freescale board, they have used 1M resistance. Can you please clarify on this?

0 项奖励
回复