Coverity issues for KW36 SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coverity issues for KW36 SDK

8,048件の閲覧回数
nsuresh2
Contributor III

Hi,

I have run the coverity for KW36 SDK and I have found 555 issues.

Please find the attached coverity report.

Let us know when these issues can be fixed? 

Thanks!

Regards,

Naven Suresh 

ラベル(1)
タグ(3)
10 返答(返信)

7,603件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi [email protected]‌,

Version of Coverity?

Aggressivity Level?

0 件の賞賛
返信

7,603件の閲覧回数
nsuresh2
Contributor III

Hi XingChang‌,

Version of Coverity: 2018.06-11

Aggressivity Level: High

Regards,

Naven Suresh.

0 件の賞賛
返信

7,603件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi Naven,

We run coverity with -agresivity level low.
Also coverity are providing "false positive findings" that in our system are marked as resolved.

0 件の賞賛
返信

7,603件の閲覧回数
nsuresh2
Contributor III

Hi XingChang‌,

The Coverity has been run already and the report is shared.

Is the Coverity results run by you are matching with our report?

If necessary, Can you run the Coverity with high aggressive level and check?

Regards,

Naven Suresh

0 件の賞賛
返信

7,603件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi Naven,

Could you please tell me, which project did you run Coverity on? I have run on ble_shell freertos and I only obtain ~270 total defects, while in the excel file there are ~550. And also could you please tell me how you have configured the analysis? (a screenshot of the Analysis Options pop-up window would be helpful)

0 件の賞賛
返信

7,603件の閲覧回数
nsuresh2
Contributor III

Hi XingChang‌,

We are running Coverity for Wireless_Uart BLE (FreeRTOS) project along with our application.

And the configuration settings are shared through the mail.

Thanks!

Regards,

Naven Suresh

0 件の賞賛
返信

7,603件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi Naven,

We try to run it according to your settings. Can you run it according to our settings?

0 件の賞賛
返信

7,603件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Let me check about this, whenever I get an update I'll let you know.

Regards,

Estephania

0 件の賞賛
返信

7,603件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi estephania_martinez‌,

Is there any update? 

0 件の賞賛
返信

7,603件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

No update yet, we are currently waiting for an official answer on this. Sorry for the inconveniences

0 件の賞賛
返信