Could some one tell me what is the System Timer Module(STM) Equivalent in S32K144.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could some one tell me what is the System Timer Module(STM) Equivalent in S32K144.

2,740 Views
sourabhbhuyan
Contributor I

Hi,

I am trying to write a small scheduler for S32K144 controller, and which needs a timer counter. Can any body tell me what is the System Timer Module(STM) Equivalent in S32K144. I can use FTM but it has only 16 bit counter and as it has other functionality like PWM generator I do not want to use it as a dedicated timer counter.

Thanks in advance.

0 Kudos
Reply
2 Replies

2,374 Views
Masmiseim
Senior Contributor I

Hey,

I don’t have any experience with this particular controller, but as it is a Cortex-M based microcontroller it must have a System-Tick-Timer:

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0179b/ar01s02s08.html

Regards

0 Kudos
Reply

2,374 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi The S32K is on preproduction, so the information is preliminary and under NDA, if you need more information about the S32K please contact your local sales to sing the NDA and get more information

Regards

Vicente Gomez

0 Kudos
Reply