Could some one tell me what is the System Timer Module(STM) Equivalent in S32K144.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could some one tell me what is the System Timer Module(STM) Equivalent in S32K144.

1,990 次查看
sourabhbhuyan
Contributor I

Hi,

I am trying to write a small scheduler for S32K144 controller, and which needs a timer counter. Can any body tell me what is the System Timer Module(STM) Equivalent in S32K144. I can use FTM but it has only 16 bit counter and as it has other functionality like PWM generator I do not want to use it as a dedicated timer counter.

Thanks in advance.

0 项奖励
回复
2 回复数

1,624 次查看
Masmiseim
Senior Contributor I

Hey,

I don’t have any experience with this particular controller, but as it is a Cortex-M based microcontroller it must have a System-Tick-Timer:

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0179b/ar01s02s08.html

Regards

0 项奖励
回复

1,624 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi The S32K is on preproduction, so the information is preliminary and under NDA, if you need more information about the S32K please contact your local sales to sing the NDA and get more information

Regards

Vicente Gomez

0 项奖励
回复