Connecting to image sensor with K series MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting to image sensor with K series MCU

Jump to solution
2,871 Views
josephchen
Contributor III

Is it possible to connect K63 to image sensor and retrieve pictures or video clips?

0 Kudos
Reply
1 Solution
2,664 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

The demo is capturing the CMOS sensor using GPIO and sending the frames to display. It is a raw image and low resolution (QVGA) and low frame rate. No video player.

If you need to play video files, video streaming, compress/encode CMOS sensor stream, etc you need to go to more powerful device with the appropriated peripheral, look at the i.Mx family.

Luis

View solution in original post

0 Kudos
Reply
3 Replies
2,664 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Check this AN:

AN4627 
AN4627, Connecting Kinetis MCU with CMOS Sensor Interface through GPIO - Application Note

Luis

2,664 Views
josephchen
Contributor III

Is it only for picture capturing or also including video clips?

Is the decompression necessary? By MCU or image sensor itself or external DSP?

0 Kudos
Reply
2,665 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

The demo is capturing the CMOS sensor using GPIO and sending the frames to display. It is a raw image and low resolution (QVGA) and low frame rate. No video player.

If you need to play video files, video streaming, compress/encode CMOS sensor stream, etc you need to go to more powerful device with the appropriated peripheral, look at the i.Mx family.

Luis

0 Kudos
Reply