Connecting to FRDM-K64F Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting to FRDM-K64F Board

2,262件の閲覧回数
Bas0037
Contributor I

Hello, I am trying to connect to my FRDM-K64F Board which has a FRDM-STBC-AGM01 Board attached to it. My goal is to use the Freedom Sensor Toolbox (CE)(v2.5.0) to run an Out of the Box Demo.

 

Originally, The device would show up on my computer as MED in the file explorer. But, would eventually show a fail text with TIMEOUT inside. The Freedom software only ever shows "waiting for a board to be connected..."

 

I followed the steps at this link to make sure the device was setup correctly: https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem...

 

I saw that the device can become corrupted when plugging into a Windows 10 device which is what I am trying to use. So, I went through the steps to update the OpenSDA at this link using the dropdown box: https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...

 

There I downloaded this Binary "DAPLink rev0244 OpenSDA v2.2 Bootloader" and proceeded with the update instructions. The drive showed up as BOOTLOADER and I pasted the downloaded binary inside. (Note: The BOOTLOADER drive did not stay up for very long inside my file explorer.). After this though when I plugged the USB back in I see no sign of connection in the file explorer or on the computer and no blinking lights on the board. I attempted to do the Bootloader steps again and the BOOTLOADER Drive would always show back up but I could still never see any sign of connection afterwards. The software also would continue to say "waiting for a board to be connected..." Is there a crucial step that I am missing to properly connect this device to my computer?

タグ(1)
0 件の賞賛
返信
1 返信

2,247件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The bootloader is not matching your firmware. You now need an external debugger(jlink) to update the bootloader. Follow the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信