Confusion using Component I2C_LDD Kinetis L

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusion using Component I2C_LDD Kinetis L

ソリューションへジャンプ
2,790件の閲覧回数
steve_fae
Senior Contributor I

If you look at typical usage for the component, you see this example below and then the prototype of the real component.  Why are they different?

3455_3455.png

But in my CW 10.3 it seems the component is different, in fact there are only 3 parameters to pass.

byte I2C2_SendBlock(void* Ptr, word Siz, word *Snt);

-Return value: Error code, possible codes:

ERR_OK - OK

ERR_SPEED - This device does not work in the active speed mode

ERR_DISABLED - Device is disabled

ERR_BUSY - The slave device is busy, it does not respond by the acknowledge (only in master mode and when interrupt service is disabled)

ERR_BUSOFF - Clock timeout elapsed or device cannot transmit data

ERR_TXFULL - Transmitter is full. Some data has not been sent. (slave mode only)

ERR_ARBITR - Arbitration lost (only when interrupt service is disabled and in master mode)

-1. parameter: Pointer to the block of data to send.

-2. parameter: Size of the block.

-3. parameter: Amount of data sent (moved to a buffer). In master mode, if interrupt support is enabled, the parameter always returns the same value as the parameter 'Siz' of this method.


ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,146件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Steven,

I think you compare methods of two different components: Internal2C component which implements SendBlock method and I2C_LDD which has MasterSendBlock. Am I right?

Best Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,147件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Steven,

I think you compare methods of two different components: Internal2C component which implements SendBlock method and I2C_LDD which has MasterSendBlock. Am I right?

Best Regards,

Lukas

0 件の賞賛
返信
2,146件の閲覧回数
steve_fae
Senior Contributor I

I figured that out after posting but couldn't find how to retract my post.  Thanks

0 件の賞賛
返信
2,146件の閲覧回数
JimDon
Senior Contributor III

Actually, you can delete your post....

Posters regret. Too bad you can't take back emails...

0 件の賞賛
返信