Hello Alberto,
Please check ENET_MSCR register in the RM of K60:
MII Speed Control Register (ENET_MSCR)
MSCR provides control of the MII clock (MDC pin) frequency and allows a preamble
drop on the MII management frame.
The MII_SPEED field must be programmed with a value to provide an MDC frequency
of less than or equal to 2.5 MHz to be compliant with the IEEE 802.3 MII specification.
The MII_SPEED must be set to a non-zero value to source a read or write management
frame. After the management frame is complete, the MSCR register may optionally be
cleared to turn off MDC. The MDC signal generated has a 50% duty cycle except when
MII_SPEED changes during operation. This change takes effect following a rising or
falling edge of MDC.
If the internal module clock is 25 MHz, programming this register to 0x0000_0004
results in an MDC as stated in the following equation:
25 MHz / ((4 + 1) x 2) = 2.5 MHz
I hope this helps.