Compile CDC VCOM example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compile CDC VCOM example

ソリューションへジャンプ
5,730件の閲覧回数
raduansarif
Contributor I

Hello,

 To transfer, data through USB, I want to compile the CDC Vcom example from MKL27Z SDK.

I don't understand how the output would be, I tried to debug this example code. I don't get any results.

Is there anyone who can give me some guidance to run this code? Thanks to everyone.

MCU: MKL27Z64LH4, IDE: MCUxpresso IDE, windows 10, I2C sensor communication

 

0 件の賞賛
返信
1 解決策
5,712件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @raduansarif ,

The CDC_VCOM example need a COM port terminal on computer. When you type any character in the terminal, the CDC_VCOM firmware can receive the character and send it back to the terminal. There is a pdf readme in example folder. You can refer to it.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,713件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @raduansarif ,

The CDC_VCOM example need a COM port terminal on computer. When you type any character in the terminal, the CDC_VCOM firmware can receive the character and send it back to the terminal. There is a pdf readme in example folder. You can refer to it.

 

Regards,

Jing

0 件の賞賛
返信
5,698件の閲覧回数
raduansarif
Contributor I

Hello, Thank you for your response.

I try to manually install the CDC-USB driver in my PC from this file (frdmkl27z_dev_cdc_vcom_bm\usb\example\usb_device_cdc_vcom\inf) but my computer reply this doesn't contain any file.

How I manually install the Virtual COM Port on my computer.

Also, the MKL27Z SDK readme file shows some links for CDC_VCOM_BM, How I will get the readme PDF file.  

Thank You

Raduan

0 件の賞賛
返信