MK64FX512VLL12 vs MK64FN1M0VLL12,Compare the two varient of Kinetis K64 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64FX512VLL12 vs MK64FN1M0VLL12,Compare the two varient of Kinetis K64 MCU

1,852 Views
punitkumar
Contributor IV

What are the things which can be done with one but not with another.

0 Kudos
Reply
2 Replies

1,441 Views
sudhanshumehta
Contributor IV

code written for 1M can run to 512 incase code written for 1M has more footprint than 512K? i am asking because 512 version has more some Flexmemory as well.

0 Kudos
Reply

1,654 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Punit.

The difference is with type of flash memory.

According to the part number MK64FN1M0VLL12 x MK64FX512VLL12

means:

M = Production

K64 = Kinetis Family K64

F = ARM® Cortex™-M4 + DSP +FPU

N = type of flash memory - Non-Flex Memory, X = Flex Memory

1M0 = 1 MB flash memory size, 512 = 512 KB

V = temperature range from - 40°C to +105°C

LL = 100 LQFP (14 mm x 14 mm) package

12 = maximum CPU frequency is 120 MHz

The difference is in flash memory (MK64FN1M0VLL12 has 1MB, MK64FX512VLL12 has 512KB) and difference with total flash memory. In addition MK64FX512VLL12 has 128 KB FlexNVM and EEPROM/FlexRAM 4KB.

K64.png

For more information please take a look at http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf

I hope this helps.

Iva

0 Kudos
Reply