Compatible with SPI 5V level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compatible with SPI 5V level

1,247 次查看
johnsonzhang1
Contributor II

pastedImage_1.png

3.3V Power for MK64FN1M0V serires MCU, The digital max input voltage can be 5.5V.

Can it compatible with 5V level SPI commmunication?

0 项奖励
回复
1 回复

1,199 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi johnson zhang ,

   From the K64 datasheet, you can find the SPI have the limited voltage range:

 pastedImage_1.png

But to the GPIO pins, all the GPIO pins is 5V tolerance.

pastedImage_2.png

Wish it helps you!


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复