Compatible with SPI 5V level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatible with SPI 5V level

1,242 Views
johnsonzhang1
Contributor II

pastedImage_1.png

3.3V Power for MK64FN1M0V serires MCU, The digital max input voltage can be 5.5V.

Can it compatible with 5V level SPI commmunication?

0 Kudos
Reply
1 Reply

1,194 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi johnson zhang ,

   From the K64 datasheet, you can find the SPI have the limited voltage range:

 pastedImage_1.png

But to the GPIO pins, all the GPIO pins is 5V tolerance.

pastedImage_2.png

Wish it helps you!


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply