My version of the jlink directory is different and does not have an erase_all_pin.jlk . I have versions:
C:\Program Files (x86)\SEGGER\JLink_V642b
and
C:\Program Files (x86)\SEGGER\JLink_V644f
Is there some other option to accomplish this task ??
---------------------------------------------
Microsoft Windows [Version 6.1.7601]
Copyright (c) 2009 Microsoft Corporation. All rights reserved.
C:\Users\Randy>cd \program files <86>\JLinkARM_V412>
The syntax of the command is incorrect.
C:\Users\Randy>cd \program files <86>\
The system cannot find the file specified.
C:\Users\Randy>cd \
C:\>cd \Program Files
C:\Program Files>cd ..
C:\>cd \Program Files <86>\segger
The system cannot find the file specified.
C:\>cd \Program Files <86>\
The system cannot find the file specified.
C:\>cd C:\Program Files (x86)\SEGGER
C:\Program Files (x86)\SEGGER>cd C:\Program Files (x86)\SEGGER\JLink_V644f
C:\Program Files (x86)\SEGGER\JLink_V644f>jlink.exe erase_all_pin.jlk
SEGGER J-Link Commander V6.44f (Compiled Apr 12 2019 17:17:37)
DLL version V6.44f, compiled Apr 12 2019 17:17:02
Unknown command line option erase_all_pin.jlk.
C:\Program Files (x86)\SEGGER\JLink_V644f>cd C:\Program Files (x86)\SEGGER\JLink
_V642b
C:\Program Files (x86)\SEGGER\JLink_V642b>jlink.exe erase_all_pin.jlk
SEGGER J-Link Commander V6.42b (Compiled Feb 5 2019 17:33:07)
DLL version V6.42b, compiled Feb 5 2019 17:31:40
Unknown command line option erase_all_pin.jlk.
C:\Program Files (x86)\SEGGER\JLink_V642b>