Code Warrior 10.6 support for MK22FN512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior 10.6 support for MK22FN512

ソリューションへジャンプ
2,090件の閲覧回数
JohnMusselman
Contributor II

Hi,

I have a project in Code Warrior 10.6 using the MK20DN512VLQ10 and I have re-spun the board to use the MK22FN512VDC12 instead.  I am trying to create a new project for the new processor, but the only choices are MK22DN..., MK22DX..., MK22FN1M0 and MK22FX512.  Does CW 10.6 support the MK22FN512??

Thanks, John

0 件の賞賛
返信
1 解決策
1,790件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello John:

K22FN512 is part of the new Kinetis devices and unfortunately it will not be supported in CodeWarrior. Instead you can migrate to KDS (Kinetis Design Studio), or one of the other supported IDEs for Kinetis. You can check the different IDEs in the next link:

IDEs for Kinetis MCUs|Freescale


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,791件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello John:

K22FN512 is part of the new Kinetis devices and unfortunately it will not be supported in CodeWarrior. Instead you can migrate to KDS (Kinetis Design Studio), or one of the other supported IDEs for Kinetis. You can check the different IDEs in the next link:

IDEs for Kinetis MCUs|Freescale


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,790件の閲覧回数
JohnMusselman
Contributor II

Thanks for the quick reply!

0 件の賞賛
返信