Clocking K64 @120MHz using 32KHz IRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clocking K64 @120MHz using 32KHz IRC?

Jump to solution
2,769 Views
nitinharish
Contributor V

Folks

Is it possible to run K64 @120MHz using 32KHz internal IRC Reference (refereed as slow clock in K64 manual) ?

1 Solution
2,506 Views
mjbcswitzerland
Specialist V

Nitin

32kHz RTC can only be used by the FLL (not by the PLL, because its value is too low for the PLL's minimum input of 2MHz).

The highest FLL factor is 2929, which limits the speed to 32768 x 2929 = 95.977472MHz

When using the FLL the USB clock should be either from IRC48M (suitable for device mode but not host) or from an external source since the FLL output is not suitable for USB (high jitter which doesn't fulfil the USB specification).

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support  / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

View solution in original post

4 Replies
2,507 Views
mjbcswitzerland
Specialist V

Nitin

32kHz RTC can only be used by the FLL (not by the PLL, because its value is too low for the PLL's minimum input of 2MHz).

The highest FLL factor is 2929, which limits the speed to 32768 x 2929 = 95.977472MHz

When using the FLL the USB clock should be either from IRC48M (suitable for device mode but not host) or from an external source since the FLL output is not suitable for USB (high jitter which doesn't fulfil the USB specification).

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support  / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

2,506 Views
nitinharish
Contributor V

mjbcswitzerland​, thanks for your blessings. I figured that out from the manual and your web page but thought you might have figured some trick out.

Thanks for the answer.

0 Kudos
Reply
2,506 Views
nitinharish
Contributor V

mjbcswitzerland, please follow me in the freescale community (that is the only way I can send you a private message).


I am interested in buying a utasker commercial license for kinetis (specially K60 and K64).

Can you please quote a price (with full support email and phone) ?

My email, I will send you in private message.

Thanks and Regards

Nitin Harish

0 Kudos
Reply
2,506 Views
mjbcswitzerland
Specialist V

Nitin

I did as you asked.

Regards

Mark

mark (at) utasker.com