Clock monitoring on KL02

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Clock monitoring on KL02

跳至解决方案
1,270 次查看
george
Senior Contributor II

Hi all,

We have planned the product using MKL02Z8VFG4.

An oscillator uses internal IRC.

And I want to share the clock to other chips.

Is it possible that it is such using KL02?

I hope that there is a pin like CLKOUT of KL05.


Or is it possible to generate the signal which is equivalent to a clock from TX using a UART block?


Do you have any ideas ?


Best Regards,

George

0 项奖励
回复
1 解答
1,093 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, George

Sorry, there is no such clock output pin in KL02. So I have to suggest you to think about KL05.

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,094 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, George

Sorry, there is no such clock output pin in KL02. So I have to suggest you to think about KL05.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复
1,093 次查看
george
Senior Contributor II

Hi, Paul,

Thank you for the reply.

OK, I study how not to use a clock output.

Best Regards,

George

0 项奖励
回复