Clock monitoring on KL02

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock monitoring on KL02

Jump to solution
1,388 Views
george
Senior Contributor II

Hi all,

We have planned the product using MKL02Z8VFG4.

An oscillator uses internal IRC.

And I want to share the clock to other chips.

Is it possible that it is such using KL02?

I hope that there is a pin like CLKOUT of KL05.


Or is it possible to generate the signal which is equivalent to a clock from TX using a UART block?


Do you have any ideas ?


Best Regards,

George

0 Kudos
Reply
1 Solution
1,211 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, George

Sorry, there is no such clock output pin in KL02. So I have to suggest you to think about KL05.

Hope my reply can help you.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
2 Replies
1,212 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, George

Sorry, there is no such clock output pin in KL02. So I have to suggest you to think about KL05.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply
1,211 Views
george
Senior Contributor II

Hi, Paul,

Thank you for the reply.

OK, I study how not to use a clock output.

Best Regards,

George

0 Kudos
Reply