Clock configuration problem with 100Mhz K20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock configuration problem with 100Mhz K20

1,712 Views
cavebiker
Contributor V

I have a K20DX256VMD10 with a 30Mhz crystal and am trying to get it to run at 96Mhz core clock.

Using Processor Expert I selected PEE MCG mode and was able to set the core clock to 96Mhz.

I generated the code with PE and placed it in the appropriate place in my K20 project.

The PE code first attempts to set up FBE mode, and that is where it hangs up, waiting for the oscillator to run, and it never does.

The PE code:

/* Switch to FBE Mode */

   /* MCG_C2: RANGE=2,HGO=1,EREFS=1,LP=0,IRCS=1 */

   MCG_C2 = MCG_C2_RANGE(0x02) | MCG_C2_HGO_MASK | MCG_C2_EREFS_MASK |  MCG_C2_IRCS_MASK;      

  /* OSC_CR: ERCLKEN=1,EREFSTEN=0,SC2P=1,SC4P=1,SC8P=0,SC16P=1 */

   OSC_CR = OSC_CR_ERCLKEN_MASK | OSC_CR_SC2P_MASK | OSC_CR_SC4P_MASK | OSC_CR_SC16P_MASK;      

  /* SIM_SOPT2: MCGCLKSEL=0 */

   SIM_SOPT2 &= (uint32_t)~(uint32_t)(SIM_SOPT2_MCGCLKSEL_MASK);                                  

  /* MCG_C1: CLKS=2,FRDIV=5,IREFS=0,IRCLKEN=1,IREFSTEN=0 */

   MCG_C1 = (MCG_C1_CLKS(0x02) | MCG_C1_FRDIV(0x05) | MCG_C1_IRCLKEN_MASK);                                  

  /* MCG_C4: DMX32=0,DRST_DRS=0 */

   MCG_C4 &= (uint8_t)~(uint8_t)((MCG_C4_DMX32_MASK | MCG_C4_DRST_DRS(0x03)));                                  

   /* MCG_C5: PLLCLKEN=0,PLLSTEN=0,PRDIV=9 */

   MCG_C5 = MCG_C5_PRDIV(0x09);                                  

  /* MCG_C6: LOLIE=0,PLLS=0,CME=0,VDIV=8 */

   MCG_C6 = MCG_C6_VDIV(0x08);                                  

  while((MCG_S & MCG_S_OSCINIT_MASK) == 0x00U) { /* Check that the oscillator is running */

   }

The red is where it hangs.

I have tried several PE clock settings and I can't get it to run past this when I select PEE for MCG mode. FEI MCG mode works fine but the core clock will only do 20+Mhz in that setting.

Any help is appreciated.

Thanks,

Tom

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,387 Views
mjbcswitzerland
Specialist V

Tom

Try removing MCG_C2_HGO_MASK (that is, set HGO=0)

Regards

Mark

1,387 Views
cavebiker
Contributor V

Hey Mark,

Your suggestion to remove  MCG_C2_HGO_MASK worked and enabled the code to run through the entire clock configuration function, thank you!. Now my code runs off to nowhere (No source available address) I will have to dig in deeper to see why that is happening.

Cheers,

Tom

0 Kudos
Reply

1,387 Views
mjbcswitzerland
Specialist V

Tom

Whether you need high gain or low power oscillator mode depends on the HW; whether there are resistors and capacitors loading it. If it is set "incorrectly" for the specific HW the oscillator may not start. and so the code hang waiting for it.

Regards

Mark

0 Kudos
Reply

1,387 Views
cavebiker
Contributor V

Thanks again Mark, I will fiddle with that stuff tomorrow and let it be known. Appreciate the help a ton!

Cheers,

Tom

0 Kudos
Reply