Changing hardware connection in CW Kinetis Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing hardware connection in CW Kinetis Project

ソリューションへジャンプ
4,084件の閲覧回数
steve_fae
Senior Contributor I

I have a project that was built with a Segger Jlink for hardware connection.  I only have access to OSBDM or a PEMicro universal multilink.  Is there a script to follow in order to modify the project settings to change the build to use what I have access to?

I am stuck at this stage.  I don't know how to import something from lets say a project that is already configured correctly.

3266_3266.png

ラベル(1)
0 件の賞賛
返信
1 解決策
3,903件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi,

The connection configuration looks ok. Do you have the two Multilik led's on?

I think you can do two things:

1) Create a new project with CW wizard and try to connect.

2) Enable log in debug connection to see what error is reported

How are you powering the TWR?

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,903件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi,

You can create a new connection like in your screen attached, completing the target device and the hardware debugger interface or just change the hw in the segger existing connection. Go to debug configurations > Select the configuration for Segger > press Edit button and in the Connection Type, select P&E instead of Jlink.

That's all.

Best Regards,

Luis

0 件の賞賛
返信
3,903件の閲覧回数
steve_fae
Senior Contributor I

Thanks Luis, I still can't connect to the target but I am sure that's because I have an LCD connected to the tower and need an external power supply.

0 件の賞賛
返信
3,903件の閲覧回数
steve_fae
Senior Contributor I

so I changed the settings from jlink to PE multilink but it won't connect

first captures shows setting second shows connection error

what i have in hand is a universal multilink but it seems to have found an FX??

3270_3270.png

3271_3271.png

0 件の賞賛
返信
3,904件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi,

The connection configuration looks ok. Do you have the two Multilik led's on?

I think you can do two things:

1) Create a new project with CW wizard and try to connect.

2) Enable log in debug connection to see what error is reported

How are you powering the TWR?

Luis

0 件の賞賛
返信
3,903件の閲覧回数
steve_fae
Senior Contributor I

Thanks, using straight usb connection with OSJTAG I got a connection.  Now need to get panel to light up.  Thanks

0 件の賞賛
返信