Changing hardware connection in CW Kinetis Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing hardware connection in CW Kinetis Project

Jump to solution
4,158 Views
steve_fae
Senior Contributor I

I have a project that was built with a Segger Jlink for hardware connection.  I only have access to OSBDM or a PEMicro universal multilink.  Is there a script to follow in order to modify the project settings to change the build to use what I have access to?

I am stuck at this stage.  I don't know how to import something from lets say a project that is already configured correctly.

3266_3266.png

Labels (1)
0 Kudos
Reply
1 Solution
3,977 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

The connection configuration looks ok. Do you have the two Multilik led's on?

I think you can do two things:

1) Create a new project with CW wizard and try to connect.

2) Enable log in debug connection to see what error is reported

How are you powering the TWR?

Luis

View solution in original post

0 Kudos
Reply
5 Replies
3,977 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

You can create a new connection like in your screen attached, completing the target device and the hardware debugger interface or just change the hw in the segger existing connection. Go to debug configurations > Select the configuration for Segger > press Edit button and in the Connection Type, select P&E instead of Jlink.

That's all.

Best Regards,

Luis

0 Kudos
Reply
3,977 Views
steve_fae
Senior Contributor I

Thanks Luis, I still can't connect to the target but I am sure that's because I have an LCD connected to the tower and need an external power supply.

0 Kudos
Reply
3,977 Views
steve_fae
Senior Contributor I

so I changed the settings from jlink to PE multilink but it won't connect

first captures shows setting second shows connection error

what i have in hand is a universal multilink but it seems to have found an FX??

3270_3270.png

3271_3271.png

0 Kudos
Reply
3,978 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

The connection configuration looks ok. Do you have the two Multilik led's on?

I think you can do two things:

1) Create a new project with CW wizard and try to connect.

2) Enable log in debug connection to see what error is reported

How are you powering the TWR?

Luis

0 Kudos
Reply
3,977 Views
steve_fae
Senior Contributor I

Thanks, using straight usb connection with OSJTAG I got a connection.  Now need to get panel to light up.  Thanks

0 Kudos
Reply