Thanks for the reply EARL,
The fact is that when we start with the project (2012) the only version that we can buy from NXP distributor was the ‘Z’ version and, until now, we always receive the ‘Z’ version from NXP.
The MK10DN512VLL10 (without ‘Z’) reference manual that you can download from the NXP website still has a bold and red inscription indicating that it is preliminary which does not give much confidence and the two parts with and without ‘Z’ are marked as ‘Active’ in the NXP status.
I think that to maintain software compatibility it would have been easier to leave an empty register when removing SIM_SOPT6 than giving an unforeseen interruption.
It seems that avoiding writing in this register the rest of the program works, but it would be necessary to review all the differences that appear in document AN4445 to be sure that we will not have problems (very hard work).
The easiest thing is to buy the version with 'Z'.