Change bootloader in ROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change bootloader in ROM

ソリューションへジャンプ
3,712件の閲覧回数
thiagopalmieri
Contributor III

Hello all,

Is it possible to edit/change the bootloader stored in ROM on a MKL43 or MKL27?

If that is possible, where can I find an example/document describing the process?

Thx

ラベル(2)
0 件の賞賛
返信
1 解決策
3,364件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Thiago Palmieri,

  No, you can't put your own bootloader in the ROM, the ROM already have the definite bootloader and can't be erased before out of factory.

If you want to use the customized bootloader, you should put it in the front of the flash, just like the old kinetis chip which don't have the ROM bootloader.

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,364件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Thiago Palmieri,

    KL43 and KL27 already have the ROM bootloader, it supports USB,I2C,SPI and LPUART peripheral interfaces, you don't need to use the flash bootloader again.

When you use the ROM bootloader, just make sure your MCU is boot from ROM,  You can check your flash address 0X40D(FTFA_FOPT), bit 7-6 indicator the boot source selection.

About the example and document, please refer to kinetis bootloader1.2.0, the link is:  www.freescale.com/KBOOT

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,364件の閲覧回数
thiagopalmieri
Contributor III

Hello Jingjing,

Yes, I know they have a default bootloader already stored in ROM.

But I want to know if it is possible to write my own customized bootloader and replace the original bootloader in ROM, is that possible? Or in case I need a customized bootloader I will need to use part of the FLASH to store it?

Thanks,

Thiago

0 件の賞賛
返信
3,365件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Thiago Palmieri,

  No, you can't put your own bootloader in the ROM, the ROM already have the definite bootloader and can't be erased before out of factory.

If you want to use the customized bootloader, you should put it in the front of the flash, just like the old kinetis chip which don't have the ROM bootloader.

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,364件の閲覧回数
thiagopalmieri
Contributor III

Yes, That is what I thought, but was hoping for a different answer.

Thanks !

0 件の賞賛
返信