Capacitors on VDDA and VREFH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Capacitors on VDDA and VREFH

1,562件の閲覧回数
pozz
Contributor III

I see two capacitors for VDDA and two capacitors for VREFH pins on TWR-K60N512. They are both X7R chip capacitors, 100nF and 10nF.

What is the reason to use two of them? Is it sufficient to use a single 100nF X7R capacitor near VDDA and VREFH pins of microcontroller?

0 件の賞賛
返信
1 返信

1,355件の閲覧回数
Dekiru
Contributor IV

They are bypass capacitors. They have different capacitance, ESR and ESL that help to eliminate the noise at different frequencies.

If you put only one, the noise at a frequency range may effects to working of the chip.

 

You can get more information if google with "bypass capacitor combination"

 

Regards

0 件の賞賛
返信