Capacitors on VDDA and VREFH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capacitors on VDDA and VREFH

1,555 Views
pozz
Contributor III

I see two capacitors for VDDA and two capacitors for VREFH pins on TWR-K60N512. They are both X7R chip capacitors, 100nF and 10nF.

What is the reason to use two of them? Is it sufficient to use a single 100nF X7R capacitor near VDDA and VREFH pins of microcontroller?

0 Kudos
Reply
1 Reply

1,348 Views
Dekiru
Contributor IV

They are bypass capacitors. They have different capacitance, ESR and ESL that help to eliminate the noise at different frequencies.

If you put only one, the noise at a frequency range may effects to working of the chip.

 

You can get more information if google with "bypass capacitor combination"

 

Regards

0 Kudos
Reply