Cannot get I2S RX DMA working on a rev 2 K10 (MK10DX256VMD10)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot get I2S RX DMA working on a rev 2 K10 (MK10DX256VMD10)

2,430件の閲覧回数
vespaman
Contributor III

I am stuck. I have a I2S mono microphone (left channel) which I want to read 32/24 bits from. Clock is up, and scope gives the data I would expect.

But, I only get '0' in my dma rx buffer when my DMA FULL interrupt arrives.

TX works just fine, but I have been fighting with RX for a long time now. I think that part of my problem is that there are no real examples, and those that I can find are for the older chip revision.

If I instead of dma request, let I2S rx generate an interrupt, I can read out data which looks alright (at least not 0) from I2S0_RDR0, so I think it is the DMA setup that I am having issues with.

buf_rx in dma setup is 32-bit aligned.

I2S rx setup:

    I2S0_RCR1 = 2;  // Water mark

    I2S0_RCR2 = I2S_RCR2_SYNC(0) | // Asynch mode

                I2S_RCR2_MSEL(1) |

                I2S_RCR2_DIV(5) |

                I2S_RCR2_BCP_MASK |

                I2S_RCR2_BCD_MASK;

    I2S0_RCR3 = 1<<16; // Enable Channel 0

    I2S0_RCR4 = I2S_RCR4_FRSZ(I2S_CONFIG_WORDS_IN_A_FRAME-1) |

                I2S_RCR4_SYWD(31) |

                I2S_RCR4_MF_MASK |

                I2S_RCR4_FSP_MASK |          // Frame active low

                I2S_RCR4_FSD_MASK;           // Frame generated internally. (Output)


    I2S0_RCR5 = I2S_RCR5_WNW(31) |

                I2S_RCR5_W0W(31) |

                I2S_RCR5_FBT(31);

    // enable RX

    I2S0_RCSR = I2S_RCSR_RE_MASK |  // enable rx

                I2S_RCSR_BCE_MASK | // enable bit clock

                I2S_RCSR_FRDE_MASK; // enable DMA requests

DMA setup:

void hal_dma_init_for_i2s_rx(unsigned int buf_rx, unsigned int block_n_sample)

{

    DMA_TCD tcd;

    DMAMUX_CHCFG2 = DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(14);

    DMA_CR |= DMA_CR_EMLM_MASK;

    DMA_CSR(2) = DMA_CSR_INTMAJOR_MASK;

    enable_irq(2);

    tcd.channel   = 2;

    tcd.nbytes    = 4; // Reading from a 32 bit register

    tcd.attr      = DMA_ATTR_SSIZE(DMA_SIZE_32_BIT) | DMA_ATTR_DSIZE(DMA_SIZE_32_BIT);

    tcd.saddr     = (unsigned int) &I2S0_RDR0;

    tcd.soff      = 0; // Do not increment

    tcd.slast    = 0;

    tcd.dadd    = buf_rx; // Destination

    tcd.doff      = 4;

    tcd.dlast_sga = 0;

    tcd.citer     = block_n_sample*2;

    tcd.biter     = block_n_sample*2;

    _dma_init(&tcd);

    // enable DMA channel

    DMA_SERQ = DMA_SERQ_SERQ(2);

}


ラベル(1)
タグ(3)
3 返答(返信)

2,071件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Micael,

I check your eDMA setting, there with some place need be modified:

DMA_CSR(2) = DMA_CSR_INTMAJOR_MASK;

need be replaced with:

tcd.csr = DMA_CSR_INTMAJOR_MASK;    //generate interrupt at end of major loop

DMA_SERQ = DMA_SERQ_SERQ(2);

need be replaced with:

DMA_ERQ |= DMA_ERQ_ERQ2_MASK;

About I2S DMA RX example, please check attached Kinetis 100MHz V2 product I2S module validation code (<sai_test.c> sai_dma_test function).


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,071件の閲覧回数
bosleymusic_com
Contributor IV

Found this post while looking through various SAI / I2S problems people have had in order to try to figure out my own hang-up. Out of curiosity is there a "verification file" for the Kinetis K22 SAI? I'm having trouble trying to get it up and running, and an example without the soundcard features like in the tower examples might help me out.

0 件の賞賛
返信

2,071件の閲覧回数
vespaman
Contributor III

Hi Ma,

Thank you for your suggestions. Unfortunately, they did not bring any change - still I get only zeroes. The DMA is actually writing zeroes to the buffer, so I am unsure if this is a matter of DMA issue or a I2S set-up issue.

Also, thank you for the example. I'll look deeper into it, since it seams to be similar to what I try to accomplish.

Regards,

Micael

0 件の賞賛
返信