Cannnot access memory of MKL26Z64VFT4 microcontroller using keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannnot access memory of MKL26Z64VFT4 microcontroller using keil

1,041 Views
dileeptn
Contributor I

hi

currently i am working on a project using MKL26Z64VFT4 micro controller. I am using jlink to program the micro controller. But i am facing an  issue right now. Keil shows "cannot access memory"  and after that "error: flash download failed - Target DLL has cancelled". The error came when i am trying to initiate loading hex file to micro controller.  Did anyone faced issue like this. Please help me regarding the issue.

Any help will be appreciated.

i am using Keil, Jlink and MKL26Z64VFT4 micro controller

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

933 Views
miduo
NXP Employee
NXP Employee

Hi,

Did you use the NXP evaluation board or only a customer board? Usually the error " Cannot access memory" caused by incorrect memory setting. Pls double check. For example check link command file which configures the SRAM and flash space for the application code and data.

0 Kudos
Reply